Other Parts Discussed in Thread: CC2650
Hi there,
I am new to the CC2650 launchpad. It's a really cool platform but a lot needs to be learned. I want use it for an RFID project specifically for low frequencies (100 - 150kHz). Is this is achievable using the CC2650? The design will use a custom analog front end module. I want to use the CC2650 to process the data obtained via the RF link and send it to a connected device(Bluetooth).
I would appreciate if you could give me some inputs on the same.
1) What will I require for the project(headers, etc?) - Does TI have any header files for RFID projects?
2) Are there any example RFID projects using TI's products, that I could take a look at?
3) Can I work on an exisitng project example or will I have to create a new project from scratch?
4) What additional information should be aware when dealing with CC2650 and RFID?
Best,
AM