Tool/software: Code Composer Studio
One gateway (CC2640r2f) is at central mode and non-expected entry Suspend. The replication process is as follows:
1. Use SDK 1.50.00.71 , define xpower_saving , running in CCS 's Debug Mode .
2. It is connection with another tag (2640r2f) which is in 1.50.00.71 Peripheral
3. Lengthen the distance between the two units until disconnected.
4. After disconnection, let the gateway (central) scan again and shorten the distance until connected.
5. Repeat 3~4 times, (<15 times ) , the Central does not response.
6.We pause at this Debug Mode , and get Call Trace as shown in the attachment file.