Other Parts Discussed in Thread: CC2640
Tool/software: TI-RTOS
Dear Team,
The following hardware and software we are using :
Part Number : CC2640R2F
SDK version : 1.50.00.58
TI-RTOS : Using RTOS in flash
Stack Image : Split Image Configuration
We are using SPI0 and SPI1 channels.
Following doubts we are having :
From
document, indicates that, If we are using RTOS in flash. then RAM will be starts from 0x20000100 if our understanding is correct. But when we are trying to compile project and checking in the Map file, then RAM was not saving any information on 0x20000100 to 0x20000520. Also not starting from 0x20000100 instead, its starting from 0x20000520.
This are the doubts we have :
- Is there any documents available to understand more about RAM allocation (0x20000000 to 0x20005000).
- Is it possible that, programmer can use reserved space of 0x20000100 Plus 264 bytes.
- Where we can find information about RESERVED RANGES which indicates reserved of the below memory locations.
- [0x20000000-0x200000c7]
[0x20000430-0x2000043f]
[0x20000440-0x2000044f]
[0x20000500-0x2000050f]
[0x20000510-0x2000051f]
[0x20004f80-0x20004f83]
[0x20004f84-0x20004f87]
[0x20004f88-0x20004f8b]
[0x20004f8c-0x20004f8f]
[0x20004f90-0x20004f93]
[0x20004f94-0x20004f97]
[0x20004f98-0x20004f9b]
[0x20004f9c-0x20004f9c]
- [0x20000000-0x200000c7]
- In one query indicates, if we are using SPI then full 512 byte table will be used, like that. that means programmer can't use the reserved space of (0x20000100 to 0x20000520) ?
- For 3 Services with 4 characteristics each, how much Heap memory is needed. Is there any document is available for us to calculate the exact heap is needed based on service and characteristics? If Yes provide link here.!
Here am providing you the below threads for your information.




Could anyone provide us suggestions on this.
Thanks for your support in advance.
Regards,
Siva.