Hi TI experts,
I am installing all BLE environments to a new laptop under Windows 10 64bit including Intel chipset Core i7 7thGen.
Launchpad is not recognized from TI Smart Programmer 2 and CCS and IAR EW. It returns -260 error.
And I realized that it is detected as XDS110(02.03.00.12) Embed with CMSIS-DAP.. So, I tried to update the related drivers to make it work as "Class Data port and Debug probe" mode.
By the way, driver updating for XDS110(02.03.00.12) Embed with CMSIS-DAP doesn't work at all.
"Access is denied" happens as below even though I run the related program as an administrator right.
By using DPInst64, I tried to solve this out, but it still has the same issue.
Of course, the boards are recognized well on my old laptop. it works well with respect to DFU, Serial number, and so on. So, firmware.bin also works well.
But, the DFU related commands always show that "0 devices" under the new environment. it doesn't detect the board at all.
BR,
Ji-won Lee