This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC2640R2-SDK: v1.50 Host Test hex file not working with BLE Device Monitor?

Part Number: SIMPLELINK-CC2640R2-SDK
Other Parts Discussed in Thread: CC2640R2F

Hi,

     I flash the SDK v1.50 host test hex file to CC2640R2F Launchpad. At BLE Device Monitor I got this error. I set the Baud Rate at 115200.

18:55:35.541 > Host: COM12 115200 baud no flowc.

18:55:35.542 > HCI log disable

18:55:35.583 > HCI_Ext_Build_Revision: status=00 Rev=0

18:55:35.584 > BLE Host TI BLE 3.0 CC2640R2

18:55:35.587 > HCI_Ext_Reset_System: status=00

18:55:36.579 > BLE host reset timeout. A hard reset may be required.

-kel