Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640
We designed a custom board using cc2640r2f with ti-launchpad as reference design.
while powering up the board the processor didnt response as well as not drawing a current of 2mA(circuit contains an LED),when we check the voltage on VDDR it shows 0-0.1V range and also DCOUPL shows 0v but as per hardware trouble shooting guide (cc26xx-HW troubleshooting-wikki) VDDR should be around 1.6V and the DCOUPL should be around 1.28.
the circuit diagram attached with this messagecc2640_p.pdf2604.cc2640.pdf