The data sheet for CC2640 shows an two antenna solution. However, the chipset is made for other radio types than BLE. Therefore i want to know if the two antenna solution can be used for BLE specific .
1)Can the two-antenna solution be used for BLE?
2)Does it make sense to use this for BLE?
3)Is the two-antenna solution supported to BLE SW?
4)How does the two-antenna solution works? Is it antenna divergence based on RSSI measurements?
BR Karsten