Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: CC2640R2F
Tool/software: TI-RTOS
Hello all
I am trying to read the Advertising data of an advertising device where i want to filter the BLE devices based on advertising data,
I am able to read address and as well as rssi of the scanned nearby BLE devices but now i want to read the Advertising data but i am not able to do so.
I have made some modification as per my understanding to read the advertising dat and snippet is attached below
Changes in " simpleobserver.c "
/*********************************************************************
* @fn SimpleBLEObserver_processRoleEvent
*
* @brief Observer role event processing function.
*
* @param pEvent - pointer to event structure
*
* @return none
*/
static void SimpleBLEObserver_processRoleEvent(gapObserverRoleEvent_t *pEvent)
{
switch ( pEvent->gap.opcode )
{
case GAP_DEVICE_INIT_DONE_EVENT:
{
Display_print0(dispHandle, 1, 0, Util_convertBdAddr2Str(pEvent->initDone.devAddr));
Display_print0(dispHandle, 2, 0, "Initialized");
// Prompt user to begin scanning.
Display_print0(dispHandle, 5, 0, "Discover ->");
}
break;
case GAP_DEVICE_INFO_EVENT:
{
SimpleBLEObserver_addDeviceInfo(pEvent->deviceInfo.addr,
pEvent->deviceInfo.addrType, pEvent->deviceInfo.pEvtData);
}
break;
case GAP_DEVICE_DISCOVERY_EVENT:
{
// Discovery complete.
scanning = FALSE;
// Copy results.
scanRes = pEvent->discCmpl.numDevs;
memcpy(devList, pEvent->discCmpl.pDevList,
(sizeof(gapDevRec_t) * pEvent->discCmpl.numDevs));
Display_print1(dispHandle, 2, 0, "Devices Found %d", scanRes);
if ( scanRes > 0 )
{
Display_print0(dispHandle, 3, 0, "<- To Select");
}
// Initialize scan index.
scanIdx = -1;
// Prompt user that re-performing scanning at this state is possible.
Display_print0(dispHandle, 5, 0, "Discover ->");
}
break;
default:
break;
}
}
/*********************************************************************
* @fn SimpleBLEObserver_eventCB
*
* @brief Observer event callback function.
*
* @param pEvent - pointer to event structure
*
* @return TRUE if safe to deallocate event message, FALSE otherwise.
*/
static uint8_t SimpleBLEObserver_eventCB(gapObserverRoleEvent_t *pEvent)
{
// Forward the role event to the application
if (SimpleBLEObserver_enqueueMsg(SBO_STATE_CHANGE_EVT,
SUCCESS, (uint8_t *)pEvent))
{
// App will process and free the event
return FALSE;
}
// Caller should free the event
return TRUE;
}
/*********************************************************************
* @fn SimpleBLEObserver_addDeviceInfo
*
* @brief Add a device to the device discovery result list
*
* @return none
*/
static void SimpleBLEObserver_addDeviceInfo(uint8 *pAddr, uint8 addrType, uint8 *pRawData)
{
uint8 i;
// If result count not at max
if ( scanRes < DEFAULT_MAX_SCAN_RES )
{
// Check if device is already in scan results
for ( i = 0; i < scanRes; i++ )
{
if (memcmp(pAddr, devList[i].addr, B_ADDR_LEN) == 0)
{
return;
}
}
// Add addr to scan result list
memcpy(devList[scanRes].addr, pAddr, B_ADDR_LEN );
memcpy(devList[scanRes].pEvtData,pRawData,B_MAX_ADV_LEN);
devList[scanRes].addrType = addrType;
// Increment scan result count
scanRes++;
}
}
Changes in " gap.c "
/********************************************************************************
/// @brief Type of device discovery (Scan) to perform.
typedef struct
{
uint8 eventType; //!< Indicates advertising event type used by the advertiser: @ref GAP_Adv_Report_Types
uint8 addrType; //!< Address Type: @ref GAP_Addr_Types
uint8 addr[B_ADDR_LEN]; //!< Device's Address
int8 rssi;
uint8 *pEvtData;
} gapDevRec_t;
/**
* @addtogroup GAP_Events
* @{
*/
//*********************************************************************************
The code gets stuck after the Instruction
"memcpy(devList[scanRes].pEvtData,pRawData,B_MAX_ADV_LEN);"
Please help me with this issue at the earliest
Thank You and Regards
Utkarash