Part Number: CC2640R2F
Hello,
I am using following for off_chip OAD
1.CC2640R2F custom board
2.external flash memory MX25R1635
3.CCS 7.4 version
4.SDK version 1.40.00.45.
I changed macro CC2640R2_LAUNCHXL_SPI_FLASH_CS from PIN_UNASSIGNED to IOID_22 in CC2640R2_LAUNCHXL.h file.
aslo i changed scan response data to"SimpleperipheOAD".
and programmed Off-Chip example program to my CC2640R2F custom board .
Using BTool I establish connection to my CC2640R2F. I select OAD to External Flash and then start the OAD Process. After completion of OAD, i restart the device and reconnect using btool and check the scan response data of my device and stil it is showing "SimplePeripheral", means the Off-Chip OAD did not happen but it is showing OAD successful.
What needs to be do to achieve a successful Off-Chip OAD?