This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Unable to increase PDU size in BLE stack

Part Number: CC2640R2F

Hello,

I have difficulties increasing the PDU size to 250.

My environment:
SDK:                       simplelink_cc2640r2_sdk_1_50_00_58
HW:                       LAUNCHXL-CC2640R2
Project:                based on simple_peripheral_cc2640r2lp_app.

At this moment I have an effective PDU size of 20 bytes.

I followed the instructions as mentioned in the header “ble_user_config.h”

When looking into the memory, I see that the bleStackConfig has been changed (maxPduSize = 0xFA)

Upon sending a databuffer with size 40 by “GATT_Notification()”, this function returns 0x1b as status.
NOTE: Sending databuffers with a size up to 20 bytes is working OK.

Q: What did I miss, how can I get this working?

Regards,
Gerrit