Other Parts Discussed in Thread: BLE-STACK, CC2650, CC2640R2F
Hi,
I'm really confused regarding some of the version number revisions of the various BLE SDKs available, and feel like the documentation is very unclear.
First of all I wanted to ask about the difference between SDK 1.40.00.45 and SDK 1.50.00.71. I know that they are not compatible and projects require quite a lot of modifications to migrate from one to another. But I want to know the main BLE functionality difference there. As per the Release notes, 1.50.00.71, supports all new features that BLE 5 introduces (Where LE Coded PHY is evaluation only) and I was told by an TI employee that this was the only SDK that was able to utilize all these new features, including LE Coded.
The SDK 1.40.00.45 Release Notes however state that "The BLE5-Stack is Bluetooth certified with the 2 Mbps feature and all Bluetooth 4.0, 4.1 and 4.2 LE core specification features from BLE-Stack v3.x. LE Coded PHY demonstration (non-production) mode for evaluating data throughput in Bluetooth 5 long range connections."
I know that the 1.50.00.71 SDK does support the LE Coded and I have demonstrated that but I don't really find any good documentation about the difference between these two SDKs.
So is the case that LE Coded can be utilized in both SDKs? Then what is the main difference between the two SDKs? How would one proceed on migrating an application currently using SDK 1.40.00.45 to use SDK 1.50.00.71?
Thanks & Regards,
Gamli