Other Parts Discussed in Thread: CC1352P
Hello!
I'm using the BLE stack (out of SDK 2.10....) on CC1352P. I want to set the output power using HCI_EXT_SetTxPowerCmd(). This works (via the RF callback, I can see that the PA is enabled or disabled, depending on the selected power), but I don't know how the supplied argument relates to the output power of the CC1352P.
I' comparing hci.h
#if defined( CC26XX ) || defined( CC13XX )
#define HCI_EXT_TX_POWER_MINUS_21_DBM LL_EXT_TX_POWER_MINUS_21_DBM //!< -21 dBm
#define HCI_EXT_TX_POWER_MINUS_18_DBM LL_EXT_TX_POWER_MINUS_18_DBM //!< -18 dBm
#define HCI_EXT_TX_POWER_MINUS_15_DBM LL_EXT_TX_POWER_MINUS_15_DBM //!< -15 dBm
#define HCI_EXT_TX_POWER_MINUS_12_DBM LL_EXT_TX_POWER_MINUS_12_DBM //!< -12 dBm
#define HCI_EXT_TX_POWER_MINUS_9_DBM LL_EXT_TX_POWER_MINUS_9_DBM //!< 9 dBm
#define HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM //!< 6 dBm
#define HCI_EXT_TX_POWER_MINUS_3_DBM LL_EXT_TX_POWER_MINUS_3_DBM //!< 3 dBm
#define HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM //!< 0 dBm
#define HCI_EXT_TX_POWER_1_DBM LL_EXT_TX_POWER_1_DBM //!< 1 dBm
#define HCI_EXT_TX_POWER_2_DBM LL_EXT_TX_POWER_2_DBM //!< 2 dBm
#define HCI_EXT_TX_POWER_3_DBM LL_EXT_TX_POWER_3_DBM //!< 3 dBm
#define HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM //!< 4 dBm
#define HCI_EXT_TX_POWER_5_DBM LL_EXT_TX_POWER_5_DBM //!< 5 dBm
with ll.h
#if defined( CC26XX ) || defined( CC13XX )
#define LL_EXT_TX_POWER_MINUS_21_DBM 0
#define LL_EXT_TX_POWER_MINUS_18_DBM 1
#define LL_EXT_TX_POWER_MINUS_15_DBM 2
#define LL_EXT_TX_POWER_MINUS_12_DBM 3
#define LL_EXT_TX_POWER_MINUS_9_DBM 4
#define LL_EXT_TX_POWER_MINUS_6_DBM 5
#define LL_EXT_TX_POWER_MINUS_3_DBM 6
#define LL_EXT_TX_POWER_0_DBM 7
#define LL_EXT_TX_POWER_1_DBM 8
#define LL_EXT_TX_POWER_2_DBM 9
#define LL_EXT_TX_POWER_3_DBM 10
#define LL_EXT_TX_POWER_4_DBM 11
#define LL_EXT_TX_POWER_5_DBM 12
and ble_user_config.c
#elif defined(CC13X2P)
// Tx Power Values (Pout, Tx Power)
const txPwrVal_t TxPowerTable[] =
{ {TX_POWER_MINUS_21_DBM, RF_TxPowerTable_DefaultPAEntry( 7, 3, 0, 3) }, // 0x000006C7
{TX_POWER_MINUS_18_DBM, RF_TxPowerTable_DefaultPAEntry( 9, 3, 0, 3) }, // 0x000006C9
{TX_POWER_MINUS_15_DBM, RF_TxPowerTable_DefaultPAEntry( 8, 2, 0, 6) }, // 0x00000C88
{TX_POWER_MINUS_12_DBM, RF_TxPowerTable_DefaultPAEntry(10, 2, 0, 8) }, // 0x0000108A
{TX_POWER_MINUS_10_DBM, RF_TxPowerTable_DefaultPAEntry(12, 2, 0, 11) }, // 0x0000168C
{TX_POWER_MINUS_9_DBM, RF_TxPowerTable_DefaultPAEntry(13, 2, 0, 5) }, // 0x00000A8D
{TX_POWER_MINUS_6_DBM, RF_TxPowerTable_DefaultPAEntry(13, 1, 0, 6) }, // 0x0000204D
{TX_POWER_MINUS_5_DBM, RF_TxPowerTable_DefaultPAEntry(14, 1, 0, 17) }, // 0x0000224E
{TX_POWER_MINUS_3_DBM, RF_TxPowerTable_DefaultPAEntry(17, 1, 0, 20) }, // 0x00002851
{TX_POWER_0_DBM, RF_TxPowerTable_DefaultPAEntry(25, 1, 0, 26) }, // 0x00003459
{TX_POWER_1_DBM, RF_TxPowerTable_DefaultPAEntry(28, 1, 0, 28) }, // 0x0000385C
{TX_POWER_2_DBM, RF_TxPowerTable_DefaultPAEntry(13, 0, 0, 34) }, // 0x0000440D
{TX_POWER_3_DBM, RF_TxPowerTable_DefaultPAEntry(17, 0, 0, 42) }, // 0x00005411
{TX_POWER_4_DBM, RF_TxPowerTable_DefaultPAEntry(22, 0, 0, 54) }, // 0x00006C16
{TX_POWER_5_DBM, RF_TxPowerTable_DefaultPAEntry(30, 0, 0, 74) }, // 0x0000941E
{TX_POWER_6_DBM, RF_TxPowerTable_HighPAEntry(46, 0, 1, 26, 7) }, // 0x8007352E
{TX_POWER_9_DBM, RF_TxPowerTable_HighPAEntry(40, 0, 1, 39, 41) }, // 0x80294F28
{TX_POWER_10_DBM, RF_TxPowerTable_HighPAEntry(23, 2, 1, 65, 5) }, // 0x80058397
{TX_POWER_11_DBM, RF_TxPowerTable_HighPAEntry(24, 2, 1, 29, 7) }, // 0x80073B98
{TX_POWER_12_DBM, RF_TxPowerTable_HighPAEntry(19, 2, 1, 16, 25) }, // 0x80192193
{TX_POWER_13_DBM, RF_TxPowerTable_HighPAEntry(27, 2, 1, 19, 13) }, // 0x800D279B
{TX_POWER_14_DBM, RF_TxPowerTable_HighPAEntry(24, 2, 1, 19, 27) }, // 0x801B2798
{TX_POWER_15_DBM, RF_TxPowerTable_HighPAEntry(23, 2, 1, 20, 39) }, // 0x80272997
{TX_POWER_16_DBM, RF_TxPowerTable_HighPAEntry(34, 2, 1, 26, 23) }, // 0x801735A2
{TX_POWER_17_DBM, RF_TxPowerTable_HighPAEntry(38, 2, 1, 33, 25) }, // 0x801943A6
{TX_POWER_18_DBM, RF_TxPowerTable_HighPAEntry(30, 2, 1, 37, 53) }, // 0x80354B9E
{TX_POWER_19_DBM, RF_TxPowerTable_HighPAEntry(36, 2, 1, 57, 59) }, // 0x803B73A4
{TX_POWER_20_DBM, RF_TxPowerTable_HighPAEntry(56, 2, 1, 45, 63) } }; // 0x803F5BB8
Thanks,
hkr