Part Number: CC2640
Our customer is evaluating the evaluation board current consumption using a current waveform analyzer.
In the test result, when CC2640 is in active mode the current is around 1.9mA.
But a periodically pulse with 5.9mA height and very short duration is observed at the same time.
In the test software, a 50ms periodically timer interrupt is enabled.
If the period setting is changed from 50ms to 100ms the current pulse period also change from 50ms to 100ms.
Is it possible this current consumption is related in the MCU hardware?