Part Number: CC2541
Other Parts Discussed in Thread: BLE-STACK
Customer is having problems connecting to newer Android phones using CC2541 running SDK 1.2.1. The CC2541 is configured as a BLE peripheral connecting to a phone or tablet acting as the central. We've suggested migrating to SDK v1.4.2 as there were improvements made to pairing with newer Android devices. Specifically “TI recommends using BLE-Stack v1.4.1 or later to ensure pairing compatibility with Android 6.0 (Marshmallow) devices”. Included below are details on the failure. Do you think migrating to SDK 1.4.1 will resolve the issue? Any other suggestions?
Customer problem analysis below:
We've traced the root cause of customers Android-specific connection issues to the LL_ProcessEvent task being blocked and missing multiple connection events and therefore the CC2541 discards the connection and a GAP_LINK_TERMINATED_EVENT happens with an error code of LL_STATUS_ERROR_CONN_FAILED_TO_BE_ESTABLISHED. This behavior seems to match the "Limit Application Processing During BLE Activity" section from the CC2541 Software Developer's Reference Guide (section 7.2.6).
However, after further investigation into exactly which task is causing the issue we were a little surprised and we're curious if this is an issue lots of devices are running into on Android. It turns out that the GAPBondMgr_ProcessEvent task is blocking the processor for multiple connection events even though the aforementioned 'Limit Application Processing During BLE Activity' seems to insinuate the TI stack layers are set up to avoid this issue (unless I am just misunderstanding the text). Regardless, the Bond Manager task blocks for ~20 ms right after the customer Android app automatically and immediately subscribes to notifications on a characteristic, and while the connection interval is still only 7.5 ms (which is automatically and unavoidably set by Android during GATT Service Discovery). This is exactly when the LL_ProcessEvent is starved and the connection termination happens. The duration of the Bond Manager task blocking is directly related to the size of the Bonded Device list (GAP_BONDINGS_MAX) and firmware was set to the seemingly default value of 10. The CC2541 firmware is configured to allow pairing and bonding but never initiates it, nor does it's GATT database have any permissions that would require pairing so we do not need the Bonded Device list at all. The vast majority of time spent in this Bond Manager task is apparently due to reading from internal flash GAP_BONDINGS_MAX number of times in gapBondMgrResolvePrivateAddr in gapbondmgr.c.
Here are some of my questions:
- Does this identification of this as the core issue make sense to you guys? Have others run up against this exact same issue? I see on the forums others have hit this same LL_ProcessEvent starvation issue but usually due to excessive UART communication and logging in their own application blocking the OS.
- Should the GAP Bond Manager task, as part of the TI SDK/stack, be allowed to block the Link Layer task and cause this connection failure or is this something the application developer needs to modify TI stack code to protect itself against?
- Reducing the size of the Bonded Device list from 10 to 1 seems to eradicate the problem since the processing/blocking time is reduced from ~20 ms to ~2ms, which gives the Link Layer task enough time to process connection events even when the connection interval is at the minimum of 7.5 ms. However, if we do not need security at all, what is the best way to remove this altogether with as little TI stack modification as possible? Setting GAP_BONDINGS_MAX to 0 results in compilation errors, but is doing that and resolving those errors the best approach? Is there a single API we can remove safely to rid ourselves of any unnecessary Bond Manager code? We still need the GAP Bond Manager task in some fashion correct?
I can provide more context or detail and logic analyzer captures with task and radio timing to illustrate the exact behavior in failure and success cases if needed to better understand the issue, just let me know!
Thanks,
Mark