This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: How do I import a sensor controller project to CCS ?



Tool/software: Code Composer Studio

I am trying to navigate my way through the "Project from Scratch" for SCS. Since it is LaunchPad oriented, and since I am using SensorTag based on 2650 and DevPack I am doing a fair bit of acrobatics to reach my goal. There is however one problem I do need some input from you TI guys with regards to IO mapping. I mapped the input to internal ADC pin to DIO25, but trying to map output pin for LED is a problem, since SCS does not offer mapping to neither DIO10 or DIO15 which are mapped to LED1 and LED2 in the schematics. I temporarily mapped it to DIO0 and manually edited scif.h and changed #define SCIF_ADC_LEVEL_TRIGGER_DIO_O_GREEN_LED 0 to #define SCIF_ADC_LEVEL_TRIGGER_DIO_O_GREEN_LED 10. Since I haven't reached building it as yet I wanted to ask if this would present any problems.

Thnaks

Avi