Other Parts Discussed in Thread: CC2640R2F, CC2640,
Hello every one,
I got the CC2640R2 LaunchPad to know if I can add the IC CC2640R2F to my projects. My goal here is stop using the USB cable and start using the Bluetooh for comunicating with my devices.
What I need is to have a new COM Port in my PC when the device is paired with. Now, my windows PC can detect the CC2640R2 LaunchPad and pair it. Also, the CC2640R2F is set as a generic access service (GATT Services). And I am blocked in this point because I can't create a new COM port.
It's my first time using bluetooth so please correct me if I am wrong.
Thank you in advance.
I am not sure what to do or learn.
My main computer
The point is that I just want to use the IC as Simple Networ Processor unit and comunicate to it using the UART, so that I just loaded the prebuit hex files for the SNP. My problem is that there are four diferent images to this and I don't know the real diferences among them, the only thing that I iknow is not all works equals.