Module designed based on the CC2640R2FRGZ, the communication distance is too short.
Generally, For transmitter / module is about 0.5dbm smaller than the evaluation board; For reception / module is about 4dbm smaller than the evaluation board; For communication distance / module is 150-200m shorter than the evaluation board.
Evaluation board performance:
The emission is about 5dBm.
The reception is about -96dbm (1M GFSK), -91dbm (2M GFSK);
The range is about 470m.
Module performance:
1, use load capacitance 12pF, frequency deviation within 20 kHz, that can meet the requirements;
2, the transmitting power is 4.6dbm (2402), 4.2dbm (2440), 4.0dbm (2480). And the evaluation board has a similar result.
3, the receiving sensitivity is about -92dbm (1M GFSK) and -87dbm (2M GFSK).
4, the test distance is about 320m.
There are several questions to be asked:
1, is the radio data gap the main reason for the difference of the final communication distance?
2, what is the performance of the antenna on the evaluation board and what parameters are better? We use the external 0.5dbi PCB antenna to test the ranging.