Other Parts Discussed in Thread: CC2640,
I'm designing a pcb for cc2650/cc2640 devices. the requirements is to have PCB antenna plus U.FL connector for external antenna. one of the antennas will be used depending on power consumption and range/performance. as the design is using a super capacitor so the main concern is to reduce consumption and increase range and performance as possible
for both options (PCB or external antenna) the antenna will be inside plastic enclosure and will be carried in user hands.
So...
- which PCB antenna shape should be used to optimize power/performance?
- I have space on the board to add differential antenna like in the cc25xx appnote (AN058), does differential antenna help reducing the power and increase performance? can i use with cc2650?
- for u.fl antenna is there any recommendation for external antenna type and shape?