Part Number: CC2642R
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1,
Using Btool 1.42.03 with a CC26X2R running the latest 2.10.00.44 CC26X2R SDK host_test FW as the central, connected to a CC26X2R running simple_peripheral example from the same SDK.
After successful passkey pairing (bond enabled, mitm enabled) during subsequent pairing attempts, I get an SMP_PAIRING_FAILED_CONFIRM_VALUE Rx error when trying to re-pair. Is there some patch to apply? I believe I should be able to re-pair with success multiple times.