Other Parts Discussed in Thread: CC2640
We have a product based on the CC2540 processor. We would like to get it certified in the EU, but there is an RX Blocking test that is required. I have been researching this and also have the CC2640, which I can connect an XDS200 to and perform the test directly from the SmartRF 7 Studio. But it is my understanding that the CC2540 does not have direct access to the radio (like you do with the CC2640), so this test cannot be accomplished with the SmartRF Studio. I am also familiar with the various RX/TX Modem tests that can be performed with the CC2540, but the RX Blocking does not appear to be implemented in those tests.
Is there a way to modify the FW to perform the RX Blocking test and report the error packet % for a given BLE frequency? I know I can get the error packet back with an HCI call, but it appears that you must be connected to a central device in order to get the info, which is lost after disconnecting the device.
Does anyone have examples on how this might be accomplished? Or is the CC2540 unable to perform this test and therefor not certifiable in the EU?
Thanks,
Harold M Lind