This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: [CC2640R2F]HCI_EXT_ModemTestTxCmd is not working in SIMPLELINK-CC2640R2-BLE5-EVAL(SDK 1.50.00.71)

Part Number: CC2640R2F

Hi All,

I have download the SDK(SIMPLELINK-CC2640R2-BLE5-EVAL) and do RF testing.

The HCI_EXT_ModemTestTxCmd seems not available anymore by BTool or HCI 
commands. We sent it after HCI_EXT_SetTxPowerCmd and the CC2640R2F does
not return any event back or any waveform on spectrum.

I just want to make sure this HCI command is available by SDK or not or there is something
I need to configure in HostTest.

Because it looks fine by using SMRART_RF to generate any waveform.


Thanks.

BR,
George Lin

  • Hi George,

    This is a known issue with the current SIMPLELINK-CC2640R2-BLE5-EVAL release. (1.50.00.71).
    These commands are not supported on this release.

    This is fixed in the upcoming maintenance release of the CC2640R2 SDK, this release will be on the web in July of 2018.
    I cannot provide any further information or exact date at this time.