Part Number: CC1352R
All,
I am using 64 bit system, copy the attached file into wireshark manually.
But can’t be used, by the way, the wireshark version is 2.6.1.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC1352R
All,
I am using 64 bit system, copy the attached file into wireshark manually.
But can’t be used, by the way, the wireshark version is 2.6.1.
AB,
Thanks. But this is not 32bit and 64bit problem.
Do you mean only wireshark 2.4x can be used for sniffer2?
If yes, that a terrible software.
By the way, now V2.4.x can't be download anymore.
Wireshark installer from: https://www.wireshark.org/#download
Hello Qian,
Yes, it is not a 32bit/64 bit problem.
I would not know if it is a terrible software or not, but our plugins were developed for this verion.
Here you can download any previous version you need.
keep in mind that all the dll files are on sdk version 1.3 and 1.4
Regards,
AB
AB,
May I know that if we have plan to use Sniffer agent 2 supporting BT 5 sniffer data capture?