This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2650: SEnsor Controller Studio

Part Number: CC2650

Tool/software: TI-RTOS

Hi,

I'm using an ADT7311 to measure temperature. I'm programing the cc2650 with sensorcontroller studio.

Sometimes I measure 0, sometimes 128 ºC and sometimes the right temperature.

Any guess what is the problem? 

I wrote the following code:

// Read the sensor1

spiBegin(SPI_POL1_PHA1, AUXIO_SPI_CSN_SS_TEMP1);

spiTx8bit(SPI_POL1_PHA1, 0x50);

spiRx16bit(SPI_POL1_PHA1; output.temp1);

spiEnd(SPI_POL1_PHA1, AUXIO_SPI_CSN_SS_TEMP1);

// Log the output data structure

rtlLogStructs(BV_RTL_LOG_OUTPUT);

// Notify the application

fwGenQuickAlertInterrupt();

// Schedule the next execution five RTC ticks from now

fwScheduleTask(2);