This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: Higher data rate with EasyLinkTxRx or PacketTxRx example

Part Number: CC2640

With CC2640 (or CC2640R2), he wants to do test of rfPacketTxRx of higher data rate (1Mbps, 2Mbps).

Current examples of EasyLinkTxRx, PacketTxRx that are included in the latest SDK only supports 250kbps.

So, is it possible to make and test high data rate mode of PacketTxRx with CC2640 (or CC2640R2)?

If it is possible, can you provide the information of how-to guide?

Thank you.

Best regards,

Hayden