This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/CC2564C: SCO establishment blocked till ACL disconnection happen

Part Number: CC2564C


Tool/software: Linux

Hello,

1. Connected with a headset device via HF profile.

2. BLE function is enabled.

3. Receive a incoming call and accept it. At the same time SCO(WBS) channel will be initiated.

4. Before establish SCO the BLE function will be firstly disabled.

5. Then the process of establishing SCO is blocked with a about 30% reproduce rate also based on this special Sennheiser headset device more easily.

I attach air sniff & FW log, help check the cause please.

Thanks.

sco establish fails.rar