Other Parts Discussed in Thread: CC2650RC, CC3200AUDBOOST
Tool/software: TI-RTOS
Hi
I am using the central bidirectional audio project for the CC2640R2 in order to connect and receive voice from a CC2650RC but I keep getting the same error when it is streaming the signal as it is shown below. This happens when I click on the MIC button for 1 or 2 seconds. The missing frames happen even if I do a fast click.
Also, this project was supposed to be used with a CC3200AUDBOOST in order to hear the audio but, how can I do it without this? The voice.py is not detecting any USB device as well.
Thanks in advance,
Guilherme Paulo