This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650: How can I write Project Zero of MSP432P401R + BOOSTXL - CC2650 using the clould tools?

Expert 2780 points
Part Number: CC2650
Other Parts Discussed in Thread: , UNIFLASH

Hello,

With the combination of BOOSTXL-CC2650MA and MSP432P401R,
how to write project zero using cloud tools?


In the resource explorer's SimpleLink BLE plug-in, there is project zero using MSP432P401R.

Software -> SimpleLink SDK Plug-in -> Examples -> Development Tools -> MSP432P401R Launchpad - Red 2.x(Red)
-> Bluetooth -> project zero -> TI-RTOS -> CCS Compiler -> project_zero

But this project zero project imported the CC2640R2 image source.
I can not replace it because CC2650's image source can not be found anywhere in the resource explorer looking for it.


The way to think about is as follows, is there a better way?

Download and install SimpleLink BLE plug-in and import CC2650's image to CCS Cloud.
or
Write using SmartRF programmer 2, and do not press firmware update.

Regards,
Da