Part Number: CC2640R2F
Hello,
Our Objective: To create project with Peripheral Role + Observer Role + OAD
Our Project Configuration:
- CC2640R2F Launchpad
- BLE 4.2 and Ble stack sdk simplelink_cc2640r2_sdk_1_50_00_58
- Code composer studio version 8.0.0
- TI Compiler version 16.9.6
Brief Approach: Made modifications in SDK Example: (simple_peripheral_offchip_oad_stack) to support Scanning along with default Advertisement and OAD feature. P.S. It is in split configuration.
Problem: Scanning not working. Advertisement and OAD are working.
Area of suspect: oad_offchip_stack, Reason: Our project in library configuration without OAD perform both advertisement and scanning.
Project Code: https://goo.gl/ZKpf55
It would be really helpful if someone from TI provide a solution to our problem as we have to ship our product by the end of August 2018 but are not able to move over this issue. Kindly guide us.
Thank you,
Madhav