Hi
I don't find any information about the accuracy of the integrated battery monitor in the CC2652R.
In the Technical Reference Manual, it I is stated that the battery voltage is measured with an "7-bit SAR-like ADC running at 125 kHz". Does that mean the accuracy is 4.3V / 2^7 = 33.5mV ?
Is the accuracy of the normal 12 Bit ADC higher? Using the 4.3V internal refrence: 4.3V / 2^(9.8) = 6mV Is this correct?
Info: I just want to measure the change of the voltage, in other words I don't care if there is an Offset.
Thanks!