Other Parts Discussed in Thread: CC2540
Hi all,
In order to use CC2540 USB Dongle (I have rev. 1.0.1) it was recommended in another thread to install SmarRF studio to get USB driver Windows 10 x64.
I did USB trace on Win 10 and this device: USB device descriptor clearly states USB VID and PID:
- idVendor Texas Instruments 0x0451
- idProduct 0x16AA
In Setup_SmartRF_Studio_7-2.10.0.exe cebal driver has the following USB PIDs:
cebal2_x64.inf
;******************************************************************************
; Models section (specifies the supported device's hardware ID)
;------------------------------------------------------------------------------
; x64-based systems
[_Models.ntamd64]
%S_DeviceDesc1% = _Install_1, USB\VID_11A0&PID_DB20 ; CC2430DB
%S_DeviceDesc2% = _Install_2, USB\VID_11A0&PID_EB20 ; SmartRF04EB
%S_DeviceDesc3% = _Install_3, USB\VID_0451&PID_16A0 ; SmartRF05EB
%S_DeviceDesc4% = _Install_4, USB\VID_0451&PID_16A2 ; CC Debugger
%S_DeviceDesc5% = _Install_5, USB\VID_0451&PID_16AB ; CC2511 USB dongle
%S_DeviceDesc6% = _Install_6, USB\VID_0451&PID_16AC ; CC2511 USB nano dongle
%S_DeviceDesc7% = _Install_7, USB\VID_0451&PID_16AD ; CC1111 USB dongle
%S_DeviceDesc8% = _Install_8, USB\VID_0451&PID_16AE ; CC2531 USB dongle
%S_DeviceDesc9% = _Install_9, USB\VID_0451&PID_16B2 ; Generic CCxxxx USB dongle
%S_DeviceDesc10% = _Install_10, USB\VID_0451&PID_16B3 ; CC2540 USB dongle
%S_DeviceDesc11% = _Install_11, USB\VID_0451&PID_16B5 ; SmartRFTrxEB
%S_DeviceDesc12% = _Install_12, USB\VID_0451&PID_16B8 ; Generic CCxxxx evaluation board
%S_DeviceDesc13% = _Install_13, USB\VID_0451&PID_16C6 ; CC2544 USB dongle
%S_DeviceDesc14% = _Install_14, USB\VID_0451&PID_16CB ; CC2538EM
It is obvious that no driver could be found for such cc2540 dongle with PID 0x16AA.
Could anyone at TI explain