This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSlite does not output BLE Addresses when run ReadPriBle command .

Other Parts Discussed in Thread: UNIFLASH, CC2650

Hello!

I use Code Composer Studio 7.2 on Linux for build firmware for CC2650 chip. I use last version of UniFlash tool to program CC2650 chip. It's GUI version works fine and i can read Primary and Secondary BLE addresses and IEEE addresses. But when i use DSlite programming tool (from archive generated in UniFlash) i cant see BLE addresses in output. I use commands:

> ./ccs_base/DebugServer/bin/DSLite flash -c user_files/configs/cc2650f128.ccxml -e -b ReadPriBle -a ReadPriBle -g log.log
DSLite version 7.2.0.2096
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: IcePick_C
Executing Startup Scripts: IcePick_C
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: Cortex_M3_0
Executing Startup Scripts: Cortex_M3_0
GEL: Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Connecting...
Running...
Success

But i can find all requested addresses in specified log file:

0x7F3816938700 5097 3 Cortex_M3_0 FLASH C: FlashProgrammerUtility::SetValueOfProperty( DeviceBlePrimary, CC:78:AB:6C:56:80 )

Can i see in terminal output of ReadPriBle command of DSLite tool?