This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: Device not going in Sleep/Shutdown mode properly.

Part Number: CC2640

Hi,

I have some queries regarding the debug mode in cc2640. i am using simple peripheral code.

1. If I put device in debug mode, then do device will go in  sleep mode if not advertising continuously and if i put device in shutdown mode then will device go in shutdown mode?

2. I have one custom cc2640 device, device is continuously taking 1.6mA current. Device is advertising for 6 sec in a periodic timer of 30 sec. I also tried to put device in sleep device stooped broadcasting but when i checked the current it showing 1.6mA. i just wanted to confirm device is going in sleep and shutdown mode. Is there any register which i can check in debug mode to verify device is going in sleep and shutdown mode properly?