This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640R2F: Bluetooth PTS test fail(GATT/SR/UNS/BI-01-C)

Part Number: CC2640R2F

Tool/software: TI-RTOS

Hello, I'm Choongbeom from i-SENS.

I checked the PTS test case(GATT/SR/UNS/BI-01-C) with simple peripheral example of "simplelink_cc2640r2_sdk_2_20_00_49" on launchpad and it's failed.

I checked GATT/SR/GAC/BV-01-C which described as an initial condition for the GATT/SR/UNS/BI-01-C on the GATT.TS.5.0.2 document. And It's failed also.

Am I missing some settings or pre-condition for the test case?

Could you please check it again?

Thanks,

Choongbeom.

  • Hello,

    The PTS suite is not run against simple_peripheral, they are scripted using host_test app in specific configurations are not intended to be reproduced stock from the SDK.

    Since our blestack (3.x) component has already been certified with the SIG you should be able to point to our listing when certifying your end product.

    Is there a reason you are running these?
  • Hello Sean,

    The test case is mandatory as a result of listing ICS.

    But you're right that I should be able to point to the certified listing and I asked about this to the certificate authority and confirmed that no need to certify the case.

    Thank you for your support.

    Thanks,

    Choongboem