Part Number: CC256XSTBTBLESW
I use the Dual-Mode Bluetooth® Stack on STM32F4 MCUs as my reference design.
What I want to do is sending data to a client but without pairing, mean connectionless mode. I know it can be done by using the advertising mode and enter the data inside the Description Data.
I have several question about it.
1. Is there an example that can be adopt to the Dual-Mode configuration by using the HCI STM32F4 all ready use?
2. If there isn't one, is it logical to use the function static int AdvertiseLE(ParameterList_t *TempParam) as its written in the PXPDemo (maybe in some other too) and plant the data inside this buffer Advertisement_Data_Buffer.AdvertisingData.Advertising_Data[n] (n represent the array I use)?
3. If I can use the above what type of advertisement I should use for connectionless, and what parameters to write specifically here GAP_LE_Advertising_Enable(BluetoothStackID, TRUE, &AdvertisingParameters, &ConnectabilityParameters, GAP_LE_Event_Callback, 0);?
4. Any article that give hints how the best way to do connectionless between client and server with low data quantity and low power usage.
Thanks
Bar.