This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640: Can't step into "stack" project using SimpleCentral example

Part Number: CC2640
Other Parts Discussed in Thread: CC1310

Tool/software: Code Composer Studio

Dear TI community,

I'm building a custom program using the example SimpleCentral as a starting point. With the SimpleCentral example there are two projects; application "app" and the stack. I need to step into the stack code but I'm not able to. Stack code is visible but I can't set a break point or evaluate variable.

Is there a compile/link thing that needs to happen to get there??

  • Using CCS  Version: 8.1.0.00011 on a win10 PC
  • XDS200 debugger
  • ble_sdk_2_02_02_25_CC2640F128 stack

Thanks,

Fred