Part Number: CC2640R2F
My device has a Xilinx Ultrascale+ and I would like to add Bluetooth in order to control this device from a phone.
What I am looking for is a simple UART interface to a Bluetooth chip. I was hoping the CC2640R2F was my solution. It is small (4 x 4 mm), I can power it from an external 1.8V regulator, and I do not need the 32.768 kHz crystal (plus, the matched BALUN from Johanson is a bonus).
However, it looks as though none of the GPIO on the CC2640R2F defalut to UART (or even SPI or I2C).
Is it true that I must externally program/configure the CC2640R2F in order enable a serial interface to an external processor?
Does TI make a small, Bluetooth 4.1 or higher chip that has a serial interface enabled by default?
Thank you.