This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC2650: Connecting Educational Boosterpack MK II with CC2650 LaunchPad

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, ENERGIA, CC2650STK

Tool/software: Code Composer Studio

I would like to hook up the Educational Boosterpack MK II with the CC2650 LaunchPad to show something on the display (that is what I am most concerned about). I was trying to find any example files or anything of that nature to get that done in CCS. I see that there are examples on Energia, but I do not want to switch platforms. The project I am currently working on i2ctmp007_CC2650STK_TI seems to already have display drivers. I believe all I really have to do to set up the LCD is update these values for the CC2650 LaunchPad/BoosterPack combo. 

#define Board_LCD_EXTCOMIN          IOID_22
#define Board_LCD_EXTMODE           IOID_28
#define Board_LCD_ENABLE            IOID_29
#define Board_LCD_POWER             PIN_UNASSIGNED
#define Board_LCD_CS                Board_SPI_DEVPK_CS
#define Board_LCD_CS_ON             1
#define Board_LCD_CS_OFF            0

Am I correct on this assumption? And if so, what do I change these values to for my board? I am unsure what each of these parameters do.