This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: CC2652R & CC2650MODA

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650

Hi,

Currently CC2650MODA is available as entire module that can be used directly for your application. From my understanding, CC2652  (currently in preview) will be replacing the CC2650. I know from previous forum post, that CC2650 and CC2652 are pin compatible. But are there any plans of releasing certified module for CC2652 (or CC1352).

Alternatively, for my application, I need a wireless processor that accepts the command from the main processor and controls the motor driver using SPI. It also needs to capture counts from hall effect sensor and needs to transmit back to the central CPU. What will be the ideal wireless processor module for this kind of application? 

Thanks,

Swapnil