This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODA: CC2564MODA

Part Number: CC2564MODA

We are using a microcontroller to generate the CC2564MODA "SLOW_CLOCK_IN".

How accurate must this frequency be?

Table 4-4 in the datasheet shows Bluetooth: +/-250PPM and ANT: +/-50PPM.

If I do the math that works out to Bluetooth: 32,768 +/- 8.192Hz  and ANT: +/-1.6384Hz.

Is this frequency accuracy a hard requirement?

Currently we have a 32,752 square wave generated from our microcontroller, is this acceptable or do we need a tighter tolerance "SLOW-CLK_IN"?