This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2640R2: tof_passive:dissconnected reason

Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: SIMPLELINK-CC2640R2-SDK

Hi All,

Please tell me the tof_passive sample program.

After discovering tof_responder from tof_initiator, connect it and it will be Dissconnected as shown below and it will be displayed as Reason: 62.

Why is it Dissconnected? What does Reason: 62 mean?

I build without changing the sample program of tof_initiator and tof_responder.

And I do not know if it is disconnected, but the tof_passive project has not been monitored yet.

Best Regards,

Ritsuo

  • Hello,

    Which version of the SDK are you using? The error 62 translates to "Connection Failed To Be Established".

    How long does it stay connected?

    Have you tried the "Non-connected ToF" option?

    Thanks,

    David
  • Hello David san,

    Thank you for comment.

    I am using SIMPLELINK-CC2640R2-SDK v2.3.00.28.

    After finding the responder on the initiator side, Disconnect is displayed immediately after pressing BTN - 1, BTN - 02 and executing Connect.

    "Connect" was displayed for a moment on the Tera terminal, but it was disconnected immediately.

    I have not tried "Non-connected ToF" yet, so I will check later.

    Best Regards,

    Takashi