Other Parts Discussed in Thread: CC2564MODNEM, CC256XQFNEM, CC2564MODAEM, CC256XCQFN-EM
HI,
now i meet a problem with 4wire UART hardware flow control.
I config the baudrate with 115200 , 8/N/1 , NO hardware flow control and then try some hci command with such cmd , and get related command complete :
18:40:54.259 Packet "HCI_Read_Local_Version_Information", Opcode 0x1001 |
18:40:54.259 -- |
18:40:54.259 Outgoing Dump: |
18:40:54.259 0000: 01 01 10 00 .... |
18:40:54.259 Incoming Dump: |
18:40:54.259 0000: 04 0e 0c ... |
18:40:54.259 Incoming Dump: |
18:40:54.259 0000: 01 01 10 00 07 00 00 07 0d ......... |
18:40:54.259 Incoming Dump: |
18:40:54.259 0000: 00 . |
18:40:54.259 Incoming Dump: |
18:40:54.259 0000: 1a . |
18:40:54.259 Incoming Dump: |
18:40:54.259 0000: 9a . |
18:40:54.259 -- |
18:40:54.259 Packet "HCI_Command_Complete_Read_Local_Version_Information_Event", Opcode 0x1001 |
18:40:54.259 Parameters: |
18:40:54.259 | Number HCI commands : 0x01 |
18:40:54.259 | Command Opcode : 0x1001 |
18:40:54.259 | Status : 0x00 (Success) |
18:40:54.259 | HCI Version : 0x07 |
18:40:54.259 | HCI Revision : 0x0000 |
18:40:54.259 | LMP Version : 0x07 |
18:40:54.259 | Manufacturer Name : 0x000d (Texas Instruments Inc.) |
18:40:54.259 | LMP Subversion : 0x9a1a |
But if i setting the flow control with hardware, i can't get any response.
Thanks!