Other Parts Discussed in Thread: CC2642R,
I too have just ran head first into this issue! I just compiled the 'simple peripheral' project and tried to put some of my custom code into the project, already at FLASH 96%, and then goes to 100%+ and fails to compile. You should not sell this as a BLE dev board Launchpad if you can't even add 100 lines of code. The CC2650R2F only has 128k of FLASH as well. What's up???
Do you guys have a pared down BLE peripheral version that allows for a few c files to be added and some more clocks?
I hate to post into Hsai's problem but I think this is what he is talking about.