Part Number: CC2650
Other Parts Discussed in Thread: BLE-STACK
Tool/software: TI C/C++ Compiler
I am using the Sensortag CC2650 + iOS App (Ti SImplelink starter). I am trying the OAD feature using an 2.1.1 version of the Sensortag and I can see all the sensor running correctly in the iOS App once I connect it to the Sensortag. Then, when I try to upload a new .bin file (.bin file given by Ti SImplelink starter application )following the section "OAD using the SensorTag iOS App" in the processors.wiki.ti.com/.../CC2650_SensorTag_User's_Guide, the app is showing the following behavior: initially the App is downloading all the code in the Sensortag, and ones it reaches 100% it shows "FW upgrade failed: device did not disconnect after programming as it should. Firmware upgrade failed, you should check battery and settings". Since I am using a fresh new battery I guess the problem is in the settings and I actually checked that I have FEATURE_OAD selected in the pre-defined name but it is still not working. I also noticed that if I manually disconnect the battery from the SensorTag after the download reaches 100% , then the App is showing "FW upgrade successful" but then I can notice that the code did not change inside the Sensortag and the old version is still running.
please tell me wither it is my sensortag stack problem or it IOS application problem ,I tried in android application after 50 or 99.97 % the application ll going to hang (it will stop it application)
please give me the solution.
Thanks & Reagards
santhosh c