If a small bluetooth module designed by CC2541 chip is fixed in a tyre of a car, will the 2.4GHz bluetooth signal be blocked absalutely in a range of 5 meters? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If a small bluetooth module designed by CC2541 chip is fixed in a tyre of a car, will the 2.4GHz bluetooth signal be blocked absalutely in a range of 5 meters? Thanks.
Hi Fredric,
Thanks for your reply. There are still three questions about C2541:
1.Can the 256KB ROM for the coding program be enough for a harsh algorithm for example, the SHA256?
2.Does the BLE4.0 have the same penetrability with the bluetooth3.0?
3.Can RSSI function in C2541 be used to measure the distance between a master and a slave?