This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/CC2640: BLE Driver for Linux

Part Number: CC2640

Tool/software: Linux

Hi all,

I am using CC2640 for making BLE connections between existed MCU and other peripherals. I tried using host test project and proper communication is happening between MCU and CC2640 over UART.

I have few questions.

1. Is there any ready made BLE driver available in Linux, so that i can make use of it and write an application on top of it.

2. Is there any ready made BLE apps in linux for testing purpose.

3. Is it possible to connect Mobile phones with CC2640 over BLE . (Not through any app).

Note: Tried to switch on Bluetooth in my iPhone (BT 4.2, LE supported), and this device is not showing in scanned devices list of CC2640.

Could you please help me.

Thank you in advance :)