This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2640R2: BLE5_Simple_peripherak Stack 2.30.00.28 user size

Part Number: LAUNCHXL-CC2640R2
Other Parts Discussed in Thread: CC2642R, LAUNCHXL-CC26X2R1

Hi,

will TI make a CC2640R2 with more flash size?

The problem is that i want to use BLE5 Stack 2.30.00.28 with Long Range but my code doenst fit on the memory.

Here is my post and i could reduce it to 83%, but i need more.

Is the CC2642R the better choice? It has 352KB of Flash memory and  the CC2640R2 has only 128KB of In-System Programmable Flash

When does the CC2642R  will  be released?