Tool/software: TI C/C++ Compiler
I want on interrupt timer do copy shift in dma
In result i want for every next interrupt get one single byte from data in dest
for example
on first interrupt
dist = 0x01;
on second
dest = 0x02;
etc...
I know that possible, if define dest as array like
static uint8 dest[1];
and in dest[0] reach wanted.
But need copy to dest as single byte
There is possible?
define LEN = 3;
static uint16 data[LEN] = {0x01,0x02,0x03};
static uint8 dest;
dmaConfig0.SRCADDRH = ((uint16)data >> 8) & 0x00FF;
dmaConfig0.SRCADDRL = (uint16)data & 0x00FF;
dmaConfig0.DESTADDRH = ((uint16)dest >> 8) & 0x00FF;
dmaConfig0.DESTADDRL = (uint16)dest & 0x00FF;
dmaConfig0.VLEN = DMA_VLEN_1_P_VALOFFIRST;
dmaConfig0.LENH = (NO_SAMPLES >> 8) & 0x00FF;
dmaConfig0.LENL = NO_SAMPLES & 0x00FF;
dmaConfig0.WORDSIZE = DMA_WORDSIZE_BYTE;
dmaConfig0.TMODE = DMA_TMODE_SINGLE;
dmaConfig0.TRIG = DMA_TRIG_T4_CH1;
dmaConfig0.SRCINC = DMA_SRCINC_1;
dmaConfig0.DESTINC = DMA_DESTINC_0;
dmaConfig0.IRQMASK = DMA_IRQMASK_ENABLE;
dmaConfig0.M8 = DMA_M8_USE_8_BITS;
dmaConfig0.PRIORITY = DMA_PRI_HIGH;
DMA0CFGH = ((uint16)&dmaConfig0 >> 8) & 0x00FF;
DMA0CFGL = (uint16)&dmaConfig0 & 0x00FF;