Part Number: SIMPLELINK-CC2640R2-SDK
Other Parts Discussed in Thread: LAUNCHXL-CC2640R2
Tool/software: TI-RTOS
Dears Sir/Madam,
I followed this topic: dev.ti.com/.../debugging_output.html
I am using CC2640R2 launchpad board.
Seems display on the console will make BLE working not properly.
When I try to connect with device, it always disconnects immediately:
And nRFconnect(Android app) says "GATT CONN FAIL ESTABLISH".
nRF Connect, 2018-12-04 SimpleBLEPeripheral (54:6C:0E:A0:45:0C) I 10:07:53.269 [Server] Server started V 10:07:53.287 Heart Rate (0x180D) - Heart Rate Measurement [N] (0x2A37) Client Characteristic Configuration (0x2902) - Body Sensor Location [R] (0x2A38) - Heart Rate Control Point [W] (0x2A39) Immediate Alert (0x1802) - Alert Level [R W WNR] (0x2A06) V 10:07:53.565 Connecting to 54:6C:0E:A0:45:0C... D 10:07:53.565 gatt = device.connectGatt(autoConnect = false, TRANSPORT_LE) (hidden) D 10:07:53.998 [Server callback] Connection state changed with status: 0 and new state: CONNECTED (2) I 10:07:53.998 [Server] Device with address 54:6C:0E:A0:45:0C connected D 10:07:53.998 [Server callback] Connection state changed with status: 0 and new state: DISCONNECTED (0) I 10:07:53.998 [Server] Device disconnected D 10:07:53.998 [Callback] Connection state changed with status: 0 and new state: CONNECTED (2) I 10:07:53.999 Connected to 54:6C:0E:A0:45:0C D 10:07:54.035 [Callback] Connection state changed with status: 62 and new state: DISCONNECTED (0) E 10:07:54.035 Error 62 (0x3e): GATT CONN FAIL ESTABLISH I 10:07:54.035 Disconnected D 10:07:54.035 [Broadcast] Action received: android.bluetooth.device.action.ACL_CONNECTED D 10:07:54.035 [Broadcast] Action received: android.bluetooth.device.action.ACL_DISCONNECTED D 10:08:02.581 gatt.close() D 10:08:02.586 wait(200) V 10:08:02.789 Connecting to 54:6C:0E:A0:45:0C... D 10:08:02.789 gatt = device.connectGatt(autoConnect = false, TRANSPORT_LE) (hidden) D 10:08:23.018 [Server callback] Connection state changed with status: 0 and new state: CONNECTED (2) I 10:08:23.018 [Server] Device with address 54:6C:0E:A0:45:0C connected D 10:08:23.019 [Server callback] Connection state changed with status: 0 and new state: DISCONNECTED (0) I 10:08:23.019 [Server] Device disconnected D 10:08:23.057 [Callback] Connection state changed with status: 0 and new state: CONNECTED (2) I 10:08:23.057 Connected to 54:6C:0E:A0:45:0C D 10:08:23.058 [Broadcast] Action received: android.bluetooth.device.action.ACL_CONNECTED D 10:08:23.080 [Callback] Connection state changed with status: 8 and new state: DISCONNECTED (0) E 10:08:23.080 Error 8 (0x8): GATT CONN TIMEOUT I 10:08:23.080 Disconnected D 10:08:23.080 [Broadcast] Action received: android.bluetooth.device.action.ACL_DISCONNECTED D 10:08:30.240 gatt.close() D 10:08:30.243 wait(200) V 10:08:30.446 Connecting to 54:6C:0E:A0:45:0C... D 10:08:30.446 gatt = device.connectGatt(autoConnect = false, TRANSPORT_LE) (hidden) D 10:08:31.047 [Server callback] Connection state changed with status: 0 and new state: CONNECTED (2) I 10:08:31.047 [Server] Device with address 54:6C:0E:A0:45:0C connected D 10:08:31.047 [Server callback] Connection state changed with status: 0 and new state: DISCONNECTED (0) I 10:08:31.047 [Server] Device disconnected D 10:08:31.075 [Callback] Connection state changed with status: 0 and new state: CONNECTED (2) I 10:08:31.075 Connected to 54:6C:0E:A0:45:0C D 10:08:31.075 [Broadcast] Action received: android.bluetooth.device.action.ACL_CONNECTED D 10:08:31.094 [Broadcast] Action received: android.bluetooth.device.action.ACL_DISCONNECTED D 10:08:31.095 [Callback] Connection state changed with status: 62 and new state: DISCONNECTED (0) E 10:08:31.095 Error 62 (0x3e): GATT CONN FAIL ESTABLISH I 10:08:31.095 Disconnected
The original code works fine with Display on UART.