Other Parts Discussed in Thread: CC2640
Tool/software: TI-RTOS
Hello,
I am in trouble with SmartRF Flash Programmer 2 ver1.7.5
When I try to flash the my custom board which uses CC2640R2F, I get the following error messages.
>Initiate access to target: XDS-L500015C.
>Create XBAL object failed: Target connect failed
>Failed to create device object.
Here is story of the problem;
- I disabled external crystal and enabled internal RC according to 'Running Bluetooth Low Energy on CC2640 without 32kHz crystal'
- I build the project and loaded to the program into the custom board in successful way.
- When I tried to flash the chip, I got the error message given in above.
- I tried the following options in SmartRF Flash Programmer and I did not work.
- Loading new firmware into customboard
- CC26XX/CC13XX Forced Mass erase
- By the way, SmartRF Flash Programmer can detect the TI's chip.
My problem is very similar to the post that I mentioned.
Also, I loaded the firmware several times to the CC2640R2F Launchpad. It seems that there is no problem flashing the CC2640R2F Launchpad.