I am attempting to OAD my image b file to some of our prototype devices.
I was given a SmartRF05 board which came pre-loaded with the image on it.
However when I was going to load image a onto our prototype I managed to have the smartrf board selected in SmartRF Flash programmer.
I have no exposure to these devices so I am not sure how to reload the image back onto the device.
I have been trying to follow the "BLE developers guide for Over-the-air-download" but am a little lost.
I should have access to all of the files which I will need (already compiled). I have no been able to get past step 4 which involves loading a .bin file via serial using SerialBootTool as I get a timeout. Reading onwards it sounds like I will need two SmartRF05 devices? I am hoping this is not the case as I do not have two.
I simply need help getting my image b back onto my SmartRF device so I can use the joystick to send the image to my CC2540s.